Beli multistage centrifugal pump di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- Ebara Pump (Ebara Corporation) Pump Centrifugal Multistage (Pompa Sentrifugal)Deskripsi:If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the luggage to the truck depending on the delivery location. * Delivery to places without parking space is not possible. * The driver will not assist in unloading.atribut:
- Electric Motor Output (kW): 0.4
- Location to Install: Indoor / outdoor
- Total Suction Head (m): -4(20°C)
- Ebara Pump Centrifugal (Pompa Sentrifugal)Deskripsi:Pompa belum termasuk motoratribut:
- Liquid Name: Clean Water
- Temperature (°C): Below 80
- Maximum Working Pressure (bar): 10
- Casing Material: Cast Iron
- Impeller Material: Bronze Casting
- Shaft Material: 403 Stainless Steel
- Ebara Pump (Ebara Corporation) Pump Centrifugal Volute Single Suction SFD Type (Pompa Sentrifugal)Deskripsi:If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the luggage to the truck depending on the delivery location. * Delivery to places without parking space is not possible. * The driver will not assist in unloading.atribut:
- Electric Motor Output (kW): 0.4
- Frequency (Hz): 60
- Installation Location: Indoor / outdoor
- Total Suction Head (m): -6(20°C)
- Voltage (V): Three-phase 200/220
- Ebara Pump Submersible DL Series (Pompa Celup)Deskripsi:Ebara memiliki range produk Submersible Pump DL yang lengkap dengan daya 0.75 -22 kW sangat cocok digunakan pada rumahan, gedung, konstruksi dan industriatribut:
- Frequency (Hz): 50
- Type: 4 Pole, air-Filled water light
- Type of Liquid Handle: Sewage, Waste Water
- Synchronous Speed (rpm): 1500
- Ebara Pump (Ebara Corporation) Pump Centrifugal Single Suction Volute S Type (Pompa Sentrifugal)Deskripsi:This product complies with the Japanese Industrial Standard (JIS B8313). It has a robust bearing structure that allows for belt drive.If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the luggage to the truck depending on the delivery location. * Delivery to places without parking space is not possible. * The driver will not assist in unloading.atribut:
- Electric Motor Output (kW): 2.2
- Frequency (Hz): 60
- Installation Location: Indoor
- Total Suction Head (m): -6(20°C)
- Type: Centrifugal pump
- Voltage (V): Three-phase 200/220
- Calpeda Pump Centrifugal (Pump Only) (Pompa Sentrifugal)Deskripsi:N - 50 HzCentrifugal pumps 1450Rpm & 2900RpmStandard MOCatribut:
- Shaft: Stainless Steel
- Mech, Seal: Carbon Ceramic
- Liquid Temperature (°C): -10 to 90
- Casing: Cast Iron
- Ebara Pump Submersible DF Series (Pompa Celup)Deskripsi:Pompa ini juga dapat disebut pompa lumpur, pompa banjiratribut:
- Frequency (Hz): 50
- Type: 4 Pole, air-Filled water light
- Type of Liquid Handle: Sewage
- Synchronous Speed (rpm): 1500
- TSURUMI MANUFACTURING Pump Centrifugal Multistage for Clean Water TVMPK Type (Pompa Sentrifugal)Deskripsi:Its excellent self-priming performance provides outstanding pumping performance. No foot valve is required, making pumping operation easy. The simple structure conforms to self-priming theory and keeps vibration and noise low. It has the limit load characteristics of a volute pump, so it will not exceed horsepower over any range of water volume.For transporting and distributing water for construction work. For irrigating rice paddies and farmland.*All products will be offered as new standard specifications. *Therefore, special accessories and special specifications are not sold here. *Please be aware of the above before placing your order. Please also note that this is a made-to-order product and cannot be returned for any reason. *All models of this product are heavy. When receiving the product, it will be delivered to the truck, and we recommend using a forklift, so please be sure to have one ready before ordering. *Please be sure to check the frequency (Hz) before purchasing. *Do not use the product outside of its specified specifications. Doing so may result in electric leakage, electric shock, fire, etc. *Do not use for drinking water. *We do not deliver to private homes (detached houses or apartment buildings).atribut:
- Suitable Liquid: Industrial water/agricultural water
- Voltage (V): Three-phase 200
- Ebara Pump Submersible DV Series (Pompa Celup)Deskripsi:Pompa ini juga dapat disebut pompa lumpur, pompa banjiratribut:
- Frequency (Hz): 50
- Type: 2 Pole, air-Filled water light
- Type of Liquid Handle: River Water, Waste Water
- Synchronous Speed (rpm): 3000
- Ebara Pump Centrifugal Close Couple End Suction Pump (Pompa Sentrifugal)atribut:
- Power (HP): 5.5
- Power (kW): 4
- Head max (m): 52.5
- Maximum Flow Rate (L/minute): 360
- Wasser Pump Centrifugal Vertical Multistage (Pompa Sentrifugal)Deskripsi:Wasser WPM Seris merupakan jenis Pompa Vertical Multi Stage , yang tersedia dengan motor standar Wasser Pump.Motor 1 phase di lengkapi degan thermal protector dan motor 2 phase harus di hubugkan dengan motor protective sesuai SNI
- Ebara Pump (Ebara Corporation) Pump Centrifugal Single Suction Volute FS Type (Pompa Sentrifugal)Deskripsi:We offer a series of 2-pole and 4-pole models that pursue compactness and light weight. Pump efficiency has been significantly improved by adopting impellers and casings that utilize our unique analytical technology. The standard specifications (water volume range, handling liquid temperature, maximum operating pressure) have been expanded from previous models, and high pressure specifications (special specifications) are also supported. This is a BPO (Back Pull Out) model that can be disassembled and inspected without removing the suction and discharge piping or heat and cold insulation. The discharge port is located at the center of the casing, and the casing has legs, making it resistant to piping loads. Safety is enhanced by installing a sealed coupling guard and protector on the exposed rotating body.If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the luggage to the truck depending on the delivery location. * Delivery to places without parking space is not possible. * The driver will not assist in unloading.atribut:
- Installation Location: Indoor
- Ebara Pump (Ebara Corporation) Pump Submersible (Pompa Celup)Deskripsi:If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the luggage to the truck depending on the delivery location. * Delivery to places without parking space is not possible. * The driver will not assist in unloading.
- Ebara Pump (Ebara Corporation) Pump Centrifugal Single Suction Volute FS Type (Pompa Sentrifugal)Deskripsi:We offer a series of compact and lightweight 2-pole and 4-pole models. The discharge port is located at the center of the casing, and the casing has legs, making it resistant to piping loads. The exposed rotor section is fitted with a sealed coupling guard and protector for added safety. For general water supply, hot and cold water circulation, industrial water, and irrigation.* We do not deliver to private homes (detached houses / apartments).
- Ebara Pump Centrifugal Self Priming Bare Shaft Type (Pompa Sentrifugal)Deskripsi:Pompa belum termasuk motoratribut:
- Liquid Name: River Water & Fresh Water
- Temperature (°C): 0-40
- Rotation: Counter clock wise when viewed from drive end
- Casing Material: Cast Iron
- Impeller Material: Cast Iron
- Shaft Material: Carbon Steel
- Bearing Type: Sealed Ball Bearing
- Impeller Construction: Semi Open
- Stuffing Box: Packing
- Ebara Submersible Pump DS Series (Pompa Celup)atribut:
- Frequency (Hz): 50
- Type: 2 Pole, air-Filled water light
- Type of Liquid Handle: Sump
- Synchronous Speed (rpm): 3000
Daftar Harga multistage centrifugal pump Terbaru November 2026
| Ebara Pump (Ebara Corporation) Pump Centrifugal Multistage (Pompa Sentrifugal) | Rp18.999.900 |
| Ebara Pump Centrifugal (Pompa Sentrifugal) | Rp16.999.900 |
| Ebara Pump (Ebara Corporation) Pump Centrifugal Volute Single Suction SFD Type (Pompa Sentrifugal) | Rp19.999.900 |
| Ebara Pump Submersible DL Series (Pompa Celup) | Rp34.999.900 |
| Ebara Pump (Ebara Corporation) Pump Centrifugal Single Suction Volute S Type (Pompa Sentrifugal) | Rp41.999.900 |
| Leo Pump Pump Centrifugal End Suction (Pompa Sentrifugal) | Rp71.999.900 |
| Calpeda Pump Centrifugal (Pump Only) (Pompa Sentrifugal) | Rp22.999.900 |
| Ebara Pump Submersible DF Series (Pompa Celup) | Rp37.999.900 |
| TSURUMI MANUFACTURING Pump Centrifugal Multistage for Clean Water TVMPK Type (Pompa Sentrifugal) | Rp73.999.900 |
| Ebara Pump Submersible DV Series (Pompa Celup) | Rp16.999.900 |
Data diperbarui pada 23/11/2026 (Harga belum termasuk PPN)



















































































































































%20Pump%20Centrifugal%20Multistage%20(Pompa%20Sentrifugal)/fjP114869559-1.jpg)
/13P107622039-1.jpg)
%20Pump%20Centrifugal%20Volute%20Single%20Suction%20SFD%20Type%20(Pompa%20Sentrifugal)/oxP114875897-1.jpg)
/owP104884896-2.jpg)
%20Pump%20Centrifugal%20Single%20Suction%20Volute%20S%20Type%20(Pompa%20Sentrifugal)/pbP114876911-1.jpg)
/bnP110226419-1.jpg)
%20(Pompa%20Sentrifugal)/9dP108042337-1.jpg)
/p2P104884902-2.jpg)
/b2P114879398-1.jpg)
/pkP104884920-2.jpg)
/roP105734996-1.jpg)
/8oP109244312-1.jpg)
%20Pump%20Centrifugal%20Single%20Suction%20Volute%20FS%20Type%20(Pompa%20Sentrifugal)/azP114872395-1.jpg)
/9nP105781347-12.jpg)
%20Pump%20Submersible%20(Pompa%20Celup)/qlP114876957-1.jpg)
%20Pump%20Centrifugal%20Single%20Suction%20Volute%20FS%20Type%20(Pompa%20Sentrifugal)/9zP114872359-1.jpg)
/1lP107622057-1.jpg)
/0iP110946018-1.jpg)
/pbP104884911-2.jpg)
%20Alkaline%20Battery%20AA%20(Baterai%20AA)/ABC%20(Battery)%20Alkaline%20Battery%20AA%20(Baterai%20AA)%20LR6%20Millenium%20Power%204B%2B2B%201pack(4%2B2pcs)/iqS000001674-4.jpg)
/WD-40%20Multi-Use%20Product%20(Pelumas%20Serbaguna)%20333ml%201pc/60S000055216-2.jpg)
/Mama%20Lemon%20Sabun%20Cuci%20Piring%20Cair%20Pouch%20(Dishwashing%20Liquid)%20Extra%20Pouch%20680ml%201pc/j1S000001685-5.jpg)
/PaperOne%20Copy%20Paper%20A4%2075gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%201box(5reams)/9uS010737354-7.jpg)
/Sinarline%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20White%201box(5reams)/meS056175806-2.jpg)
/monotaro_id%20Kantong%20Plastik%20Sampah%20Hitam%20HDPE%2070micron%20(Trash%20Bag%20%2F%20Kresek)%201kg%2090x120cm%201pack(%C2%B17pcs)/bnS034771419-7.jpg)
/monotaro_id%20Kain%20Lap%20Mikrofiber%2040x40cm%20320gsm%20(Cleaning%20Cloth)%20Biru%20Muda%201pc/ntS034715857-3.jpg)

/Sunlight%20Sabun%20Cuci%20Piring%20Pouch%20(Dishwashing%20Liquid)%20Lime%20370ml%201pc/j8S032839692-2.jpg)
%20Alkaline%20Battery%20AAA%20(Baterai%20AAA)/ABC%20(Battery)%20Alkaline%20Battery%20AAA%20(Baterai%20AAA)%20LR03%20Milenium%20Power%204B%2B2B%201pack(4%2B2pcs)/4kS028113164-2.jpg)

/Max%20Stapler%20Needle%20(Isi%20Staples)%20No_10-1M%205%2F16x3%2F16Inch%201pack(20pcs)/S000005230-4.jpg)
/Kenko%20Cutter%20Refill%20Blade%20(Isi%20Mata%20Pisau)%20L-150%20100x18mm%201pack(5pcs)/2gS000021088-3.jpg)
/monotaro_id%201%20inch%20Clear%20Tape%20(Solasi%20%2F%20Selotip)%2064m%20Transparent%2024mmx72yard%201roll/96S042206330-1.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sarung%20Tangan/Sarung%20Tangan%20Sekali%20Pakai/Sarung%20Tangan%20PVC%20Sekali%20Pakai/Bagus%20Plastic%20Gloves%20(Sarung%20Tangan)/Bagus%20Plastic%20Gloves%20(Sarung%20Tangan)%20W-22599%2010%C2%B5%201pack(50pcs)/jsS039716712-1.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Masker/Masker%20Sekali%20Pakai/Masker%20Daily/Suojella%203ply%20Earloop%20Rubber%20Mask/Suojella%203ply%20Earloop%20Rubber%20Mask%20White%201box(50pcs)/9pS031693349-2.jpg)
/Sinarline%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20White%201ream/lyS056175790-3.jpg)
/Sinarline%20Copy%20Paper%20A4%2075gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20White%201ream/msS056175820-3.jpg)
/monotaro_id%20Lakban%20OPP%202inch%20(Solasi%20%2F%20Selotip)%20Transparent%2048mmx64m%201roll/h7S036166619-4.jpg)
/monotaro_id%20Plas%20Chamois%20(Lap%20Kanebo)%20with%20tube%20Yellow%2032x21cm%201pc/4uS037754174-2.jpg)
/monotaro_id%20Kain%20Lap%20Mikrofiber%2035x35cm%20300gsm%20(Cleaning%20Cloth)%20Biru%20Tua%201pc/65S039548221-2.jpg)
/Paperline%20Envelope%20(Amplop)%20PPL%20EV%2090%20PPS%20Buklet%20Putih%20110x230mm%201box(100pcs)/66S000008222-6.jpg)
/3M%20Red%20Buffer%20Pad%205100%20(Pad%20Buffer%20Lantai)%2016inch%201pc/3cS033966120-1.jpg)
/Standard%20Pen%20AE-7%20(Pulpen%20%2F%20Bolpoin)%20ATK02092%20Alfa%20Tip%20Black%200_5mm%201pc/dzS034610503-1.jpg)